Large bed, small van
Inevitably the key question arises: how do you get the bed in and out of the van? The solution requires both a correspondingly high lifting capacity and the entire space of the loading area. A conventional tail lift would be too small and the beds would rest on the loading edge or fall off. In addition, the tail lifts of small vans can usually only carry a maximum payload of 500 kg. Clemens Hohensulz, Managing Director of Anylift, explains the solution: “We use 90 percent of the loading area inside the van along with a movable, double floor that holds the secured cargo. When the vehicle is stationary, this floor can be mechanically extended and lowered.” The payload of the Anylift Eco variant can be up to 1,000 kg, which makes it perfect for the requirements of bed transport.
Safe loading
Markus Burdis, Operations Manager at Arjo: “We used to load the beds into the vehicles using a special rail system. However, this repeatedly resulted in damage to the bed casters. Furthermore, the whole process was very time-consuming, as beds vary in width and size. Also, the fifth wheel (drive wheel) in the center of the bed was continuously the source of difficulties when loading and unloading. Lifting platforms were also not the ideal solution due to the frequent presence of slopes. This even led to dangerous scenarios where beds would fall because they couldn't be properly secured on the platform. All of this has changed now. With Anylift, loading is reliable and safe. The load can be secured conveniently and ergonomically outside the vehicle." This is a huge advantage for the operators, who previously had to climb into the cramped cargo space of the vehicle to secure the load.